Supercapacitors with very high capacitance values and low voltages are the bridge between the capacitors and the batteries. They are mainly used as back-up devices for the power shut-down of microcomputers and RAMs, smart meters, POE network devices, alarm systems, etc.
In this webinar, KEMET's Roya Nikjoo (Field Application Engineer, Europe Nordic) explains which parameters need to be defined before choosing the right supercapacitor for your application.