CONTACT US  |  CUSTOMER SERVICE
Search Help
Search Help
click for home pageclick for productsclick for newsclick for CapacitorEdgeclick for myKEMETclick for customer serviceclick for about usclick for investor relations

KEMET NetList Files - SIMPLIS/(SIMetrix)



SIMetrix/SIMPLIS simulation software (link to Simplis web site: http://www.simplistechnologies.com/)

Once you have downloaded the model files, you may install them in SIMetrix/SIMPLIS just like you would a MOSFET or Diode model. Just drag and drop the file icon (.ckt file extension) into the SIMetrix/SIMPLIS command shell window. Click the OK button on the resulting dialog box confirming that you want to install this model in the Model Library. You can then place the new capacitor on a schematic using the "Place | From Model Library | Capacitors" menu option.

These files (*.ckt) contain element values of a prescribed network, whose artwork may be seen in associated JPEG (*.jpg) or AutoCAD Symbol library files (*.slb). These files may be downloaded from the KEMET Spice web page.

Unique to these files is the second comment line defining the capacitor as polar:
*#ASSOC symbol=cap_polar_us category=Capacitors simulator=simetrix|simplis
or as non-polar::
*#ASSOC symbol=cap category=Capacitors simulator=simetrix|simplis

Here is a Notepad view of one of the film capacitor model/file:




This is a non-polar capacitor type of 10 nF capacitance rated at 100 VDC.

The files are collected in groups and compressed in Zip files. The 1st group “KEMET MLCC C0201-C0805” consists of the ceramic chips or part types including C0201, C0402, C0603, and C0805, while the second group, "KEMET MLCC C1206-C2225", contains C1206, C1210, C1632, C1812, C1825, C2220, and C2225. These include all dielectrics: C0G, X5R, X7R, Y5V, and Z5U, where applicable.



The KEMET Alum-Polymer AO SMD Capacitors are contained in the following ZIP file:
KEMET Alum-Poly A700.zip



The tantalum commercial SMD capacitors, with MnO2 cathode systems include the standard T491, T494 (lower ESR by test version), T495 (lower ESR by design), T496 (internally fused for fail-safe), T497 (high reliability), T498 (+150°C operation), T499 (+175°C operation), and T510 (ultra-low ESR by multiple anodes).
KEMET Tant-Comm MnO2 SMD Capacitors.ZIP



Military versions of the Tantalum-MnO2 devices include T4x9 [T409 (CWR09), T419 (CWR19), T429 (CWR29)], T492 (CWR11), and T493 (COTS) capacitor types.
KEMET Tant-Military MnO2 COTS-CWR09-11-19-29.ZIP



For lower ESR devices, a conductive-polymer is used in place of the MnO2 cathode system, achieving ESRs down below 10 milliohms. These include types T520 (ESRs down to 4.5 milliohms, maximum temperature to 85°C), T525 (extended temperature range to +125°C), T521 (new higher voltage from 20Vdc to 35Vdc), T528 (facedown package with ESLs approaching 100pH, and higher ripple capability), and T530 (higher capacitance but ultra-low ESRs down to 3 milliohms, and temperature range to 125°C).
KEMET Tant-Polymer KO SMD Capacitors.ZIP



Most recently added is the surface-mount film capacitors. These are divided by dielectric types: PEN, PET, PPS, and Paper. The PEN are the polyethylene naphthalate with a temperature capability from -55°C to 150°C(125° is standard). These are characterized with dielectric constant of 3.0, minimum thickness of 1.4 um, typical dissipation factor of 0.4%, and a dielectric absorption rating of 1.2%. These include part types with series designations of GMC, GMW, and GPC.
KEMET PEN Film GMC-GMW-GPC.zip



The PET are the polyester film capacitors with a temperature capability of -55°C to 125°C(100°C is standard). These are characterized with dielectric constant of 3.3, minimum thickness of 0.9 um, typical dissipation factor of 0.5%, and a dielectric absorption rating of 0.5%. These include part types with series designations of MMC for the surface mount capacitor and MDC, MDK, and MDS for the DIL surface mount packages.
KEMET PET Film MMC-MDC-MDK-MDS.ZIP



The PPS are the polyethylene sulfide with a temperature capability from -55°C to 150°C(125° is standard). These are characterized with dielectric constant of 3.0, minimum thickness of 1.2 um, typical dissipation factor of 0.06%, and a dielectric absorption rating of 0.01%. These include part types with series designations of SPC, SMC, and SMW.
KEMET PPS Film SMC-SMW-SPC.ZIP



The metalized Paper types are limited to the single series: SMP253. These are high-voltage capacitors explicitly designed for class Y2 EMI filtering. The voltage rating for these capacitors is 250 VAC, whereas all other capacitor types have their voltage ratings expressed as VDC.
KEMET Paper SMP253.ZIP



Following is from joint press release from KEMET and Simplis:

KEMET’S PRODUCT LIBRARY AND CAPACITOR MODELS ARE NOW AVAILABLE ON THE SIMETRIX/SIMPLIS SIMULATION TOOL

Greenville, South Carolina (February 17, 2009) – KEMET Corporation (KEME.OB), The Capacitance Company, announced that it has released its full line of capacitor models to the SIMetrix/SIMPLIS simulation software, which allows Signal Integrity, Power Integrity, and board design engineers to model the decoupling scheme of a printed circuit board using the SIMetrix/SIMPLIS simulation software. KEMET’s new low ESR and low ESL polymer products are specifically designed for the high speed processor board level decoupling applications.

Using the SIMetrix/SIMPLIS simulation tool, design engineers will have the ability to model the time-domain and frequency behavior of Aluminum, Film, Ceramic, and Tantalum SMD capacitors manufactured by KEMET. This new resource will make it easier for the products of tomorrow to be designed using KEMET capacitors. KEMET has modeling software, Spice, which is available on its website kemet.com. Spice is a freeware product that aids design engineers by analyzing the performance of capacitors.

“KEMET’s goal is to get our models to perform with the most accepted, demanding, and accurate simulation software tools and we believe that we accomplish this goal with tools created by SIMetrix/SIMPLIS,” stated John D. Prymak, Director Advanced Applications, KEMET Electronics Corp. “Our focus continues to be on partnering with design engineers and helping to find the right capacitance solutions to accomplish their project’s specific need,” continued Prymak.

“SIMPLIS is the industry leading simulation tool that assists designers in figuring out how many and what type of output capacitors they need to address their customer’s application requirements,” stated Tom Wilson, President, SIMPLIS Technologies, Inc. “By taking this need seriously, and providing such high quality simulation models for their capacitors, KEMET is providing designers with extremely helpful information that will allow them to optimize their designs for cost and performance,” continued Wilson.

KEMET Corporation (KEME.OB) applies world-class service and quality to deliver industry-leading, high-performance capacitance solutions to its customers around the world. KEMET offers the world's most complete line of surface-mount and through-hole capacitor technologies across tantalum, ceramic, film, aluminum, electrolytic, and paper dielectrics. Additional information about KEMET can be found at http://www.kemet.com
NOTIFY ME OF CHANGES.
www.kemet.com News Products myKEMET Customer Service CapacitorEdge About US Investor Relations Site Help Site Map Legal Disclaimer Privacy Policy www.kemet.com