KEMET NetList Files - NetList
The files are collected in groups and compressed in Zip files. The CKT files are available in the same format as the previous NetList files as the file closing line is ".END", as well as NetList files with the closing line ".ENDS" , and the CIR files which use ".ENDS" as the closing line in each model file, and are of the filetype "CIR" - other than these two variations, they are exactly alike. Although convention has the closing line as ".ENDS", we are maintaining the ".END" closing line format as we never had complaints when we released these models, and suspect a conversion or exception was created to handle them.
The 1st compressed file ("Ceramic SMD 0201-0805 CKT.zip" - 980 models) in each row consists of the surface mount ceramic or MLCC part types “C0201-C1206” including C0201, C0402, C0603, and C0805. The second file ("Ceramic SMD 1206-2225 CKT.zip" - 1,695 models) for each row consists of the surface mount ceramic or MLCC part types "C1206, C1210, C1632, C1812, C1825, C2220, and C2225". These include all dielectrics: C0G, X5R, X7R, X8L, X8R, Y5V, and Z5U, where applicable, and now include the C0G high voltage and high temperature (200°C) chips. The third compressed file of each row contains the 0612 Arrays, listed as "CA064" part types with C0G and X7R dielectrics (73 files). The 4th file in each row contains the recently released KPS product files (180 models). The 5th compressed file in each row holds the military or the DSCC 0302x and CDR0 and CDR3 part types (458 models).
CKT File Types (CKT file uses ".END" as closing line):
    
CKT File Types (CKT file uses ".ENDS" as closing line):
    
CIR File Types:
   
The aluminum-polymer capacitor (A700) files are contained in a separate zip file. There are 121 files corresponding to 121 unique part types in this compressed file.
CKT File Types (CKT file uses ".END" as closing line), CKT File Types (CKT file uses ".ENDS" as closing line), then the CIR File Types:
 
The tantalum commercial SMD capacitors, with MnO2 cathode systems include the T491 (371 files), T494 (lower ESR by test version - 371 files), T495 (lower ESR by design - 330 files), T496 (internally fused for fail-safe - 104 files), T497 (high reliability - 130 files), T498+9 (T498 at +150°C operation and T499 at +175°C operation -149 files), and T510 (ultra-low ESR by multiple anodes - 29 files).
CKT File Types (CKT file uses ".END" as closing line):
      
CKT File Types (CKT file uses ".ENDS" as closing line):
      
CIR File Types:
      
Military versions of the Tantalum-MnO2 devices include T4x9 (T409/CWR09, T419/CWR19, T429/CWR29 - 337 files)], T492 (CWR11 - 56 files), and T493 (COTS - 440 files) capacitor types.
CKT File Types (CKT file uses ".END" as closing line):
  
CKT File Types (CKT file uses ".ENDS" as closing line):
  
CIR File Types:
  
Tantalum with conductive-polymers (for lower ESR and non-ignition failures) include the capacitor types T520 (polymer rated to +105°C - 375 files), T521-5 (T521 are high voltage polymers >16 Vdc and T525 are rated to +125°C - 44 files), T528 (facedown for low ESL and higher ripple current - 38 files), and the T530 (ultra-low ESR using multiple anodes and conductive polymer rated to +125°C - 55 files).
CKT File Types (CKT file uses ".END" as closing line):
  
CKT File Types (CKT file uses ".ENDS" as closing line):
  
CIR File Types:
  
Most recently added is the surface-mount film capacitors. These are divided by dielectric types: PEN, PET, PPS, and Paper. The PEN are the polyethylene naphthalate with a temperature capability from -55°C to 150°C(125° is standard). These are characterized with dielectric constant of 3.0, minimum thickness of 1.4 um, typical dissipation factor of 0.4%, and a dielectric absorption rating of 1.2%. These include part types with series designations of GMC, GMW, and GPC (555 files) and the LDE series (69 files).
CKT File Types (CKT file uses ".END" as closing line):
 
CKT File Types (CKT file uses ".ENDS" as closing line):
 
CIR File Types:
 
The PET are the polyester film capacitors with a temperature capability of -55°C to 125°C(100°C is standard). These are characterized with dielectric constant of 3.3, minimum thickness of 0.9 um, typical dissipation factor of 0.5%, and a dielectric absorption rating of 0.5%. These include part types (1,005 files) with series designations of MMC for the surface mount capacitor and MDC, MDK, and MDS for the DIL surface mount packages.
CKT File Types (CKT file uses ".END" as closing line):
 
CKT File Types (CKT file uses ".ENDS" as closing line):
 
CIR File Types:
 
The PPS are the polyethylene sulfide with a temperature capability from -55°C to 150°C(125° is standard). These are characterized with dielectric constant of 3.0, minimum thickness of 1.2 um, typical dissipation factor of 0.06%, and a dielectric absorption rating of 0.01%. These include part types with stacked multilayer film chip capacitors (1206, 1210, and 1812 - 35 files) and older SMD variations of SPC, SMC, and SMW (498 files).
CKT File Types (CKT file uses ".END" as closing line):
 
CKT File Types (CKT file uses ".ENDS" as closing line):
 
CIR File Types:
 
The metalized Paper types are limited to the single series: SMP253. These are high-voltage capacitors explicitly designed for class Y2 EMI filtering. The voltage rating for these capacitors is 250 VAC, whereas all other capacitor types have their voltage ratings expressed as VDC. There are 7 files in each of these compressed file.
CKT File Types (CKT file uses ".END" as closing line), CKT File Types (CKT file uses ".ENDS" as closing line), and CIR File Types:
  
|