CONTACT US  |  CUSTOMER SERVICE
Search Help
Search Help
click for home pageclick for productsclick for newsclick for CapacitorEdgeclick for myKEMETclick for customer serviceclick for careersclick for investor relations

KEMET NetList Files - Cadence

The Cadence files are based on an overly simplified RLC circuit, with values loaded for these elements from three file types: all ASCII files defined as “DCL” files containing a group of part numbers, “TXT” files defining the model package; and finally, the “DML” file that defines the electrical model elements.

Because these files are simplified to single RLC components, creating these files for electrolytic capacitors would create enormous errors and as such, the files created for these models is restricted to ceramic and film capacitors. In addition, although the KPS series capacitors do fit this modeling, they are with "J-Type" leadframe that makes them very different, but we elected to add these to the created models.

The previous offering of the Cadence models were restricted to two very large groups: ceramics and film. These are now broken into smaller groups, with smaller "DML" files that may be more representative of your requirements. The ceramics are broken into groups by dielectric, and if this group was still considerably large it was broken down into smaller groups by chip size.


Contained within the compressed file for the ceramic capacitors are corresponding 'TXT' files for each part type. The compressed files are broken into dielectric, and size categories. Additionally, high voltage (500 V through 3 kV) and high temperature (200°C capability) are separated from the standard dielectric and size offerings.

The 'DCL' group files are created for common size and dielectric (e.g., cap_kemet_ceramic_c0g_c0805.dcl, cap_kemet_ceramic_c0g_hivolt_c0805.dcl, cap_kemet_ceramic_x7R_c1206.dcl, etc.), and these files contain a lising of the TXT files included in this particular group. For each DCL file, a corresponding DML file exists defining the capacitance and parasitic elements of resistance and inductance for all part types [cap_kemet_ceramic_x7r_c0805.dml].

First is a collection of the C0G files:

Cadence KEMET Ceramic C0G HiVolt 0805-2225.zipCadence KEMET Ceramic C0G HiTemp 0603-2225.zipCadence KEMET Ceramic C0G Capacitor Arrays.ZIPCadence KEMET Ceramic C0G 1206-2225 Capacitors.zipCadence KEMET Ceramic C0G 0201-0805 Capacitors.zipCadence KEMET Ceramic C0G MIL CDR.zip

(283 PNs in C0G 0201-0805, 224 PNs in C0G 1206-2225, 42 PNs in C0G Capacitor Arrays, 443 PNs in C0G 0603-2225 HiTemp, 660 PNs in C0G HiVolt 0805-2225, and 234 PNs Military DSC0302x, CDRx)



Next is a collection of the X5R and X7R part types:

Cadence KEMET Ceramic X7R KPS LF Capacitors.zipCadence KEMET Ceramic X7R Capacitor Arrays.ZIPCadence KEMET Ceramic X7R 1206-2225 Capacitors.zipCadence KEMET Ceramic X7R 0402-0805 Capacitors.zipCadence KEMET Ceramic X5R 0201-1210 Capacitors.zipCadence KEMET Ceramic X7R MIL DSCC CDR.zip

(119 PNs in X5R 0201-1210, 175 PNs in X7R 0402-0805, 388 PNs in X7R 1206-2225, 33 PNs in X7R Capacitor Arrays, 180 PNs in X7R KPS, and 248 PNs in X7R Military DSC0302x, CDRx)


The final grouping from ceramics includes the X8L, X8R, Y5V, and Z5U dielectric collections:

Cadence KEMET Ceramic X8R C0402-C1812.zipCadence KEMET Ceramic X8L C0402-C1812.zipCadence KEMET CeramicY5V C0603-C1210.zipCadence KEMET Ceramic Z5U C0805-C2225.zip

(60 PNs in X8L 0402-1812, 157 PNs in X8R 0402-1812, 107 PNs in Y5V 0603-1210, and 89 PNs in Z5U 0805-2225)



As with the ceramic, the film (and paper) models are now broken into smaller segments to enable selection of smaller data modules. For the film (and paper) capacitors these files were separated by dielectric type, then by series type [e.g., GMC, GMW, GPC, and LDE PEN dielectrics]. The individual text files are by part kemet part numbering [e.g., "gmc10.2_224k63a31.txt"]. Except for the "PET MDx" capacitors, each compressed file will also contain one collection or DCL file [e.g., "cap_kemet_film_gmc.dcl"] and a model file ["cap_kemet_film_gmc.dml"]. The "PET Mdx" compressed files contain three collection files (MDC, MDK, and MDS) and three corresponding model files.

Cadence KEMET Film PEN GPC Capacitors.zipCadence KEMET Film PEN GMW Capacitors.zipCadence KEMET Film PEN GMC Capacitors.zipCadence KEMET Film PEN LDE Capacitors.zip

(288 PNs in PEN GMC, 112 PNs in PEN GMW, 155 PNs in PEN GPC, and 69 PNs in PEN LDE)


Cadence KEMET Film PET MDx Capacitors.zipCadence KEMET Film PET MMC Capacitors.zip

(335 PNs in PET MMC, and 370 PNs in PET MDx)


Cadence KEMET Film PPS SMC Capacitors.zipCadence KEMET Film PPS LDB Capacitors.zipCadence KEMET Film PPS SWM Capacitors.zipCadence KEMET Film PPS SPC Capacitors.zip

(35 PNs in PPS LDP 1206-1812, 242 PNs in PPS SMC, 178 PNs in PPS SMV, and 178 PNs in PPS SPC)

Cadence KEMET Paper SMP Capacitors.zip

(7 PNs in Paper SMP)


NOTIFY ME OF CHANGES.
www.kemet.com News Products myKEMET Customer Service CapacitorEdge Careers Investor Relations Site Help Site Map Legal Disclaimer Privacy Policy www.kemet.com