Skip Ribbon Commands
Skip to main content

KEMET Introduces New Aluminum Electrolytic Capacitors Series

Greenville, South Carolina (March 6, 2012) – KEMET Corporation (NYSE: KEM), a leading manufacturer of tantalum, ceramic, aluminum, film, paper and electrolytic capacitors, today introduced its new line of surface mount and miniature radial aluminum electrolytic capacitors.

These capacitors are available in a variety of configurations, and are well-suited for common applications in the industrial, lighting, consumer and alternative energy markets. Three low-profile surface mount series are offered in voltages up to 450 VDC including low impedance models with up to 5,000 hours life at 105ºC. Seven radial-lead versions are available with up to 10,000 hours life and voltages to 500 VDC. Several of these series also offer high ripple current capability for more demanding applications.

“Our latest electrolytic portfolio fulfills the need for miniature capacitors in a wide range of applications and industries,” said Andrew Bellavia, KEMET Director of Product Marketing for Film and Electrolytic Capacitors, Americas. “KEMET's electrolytic products now span the complete range from surface mount devices to large screw terminals. This allows designers the ability to select the capacitance solution with the right mix of characteristics to meet their specific requirements, even in the most demanding applications.”

For more information, please visit


KEMET’s common stock is listed on the NYSE under the symbol “KEM.” At the Investor Relations section of our web site at, users may subscribe to KEMET news releases and find additional information about our Company. KEMET applies world class service and quality to deliver industry leading, high performance capacitance solutions to its customers around the world and offers the world’s most complete line of surface mount and through-hole capacitor technologies across tantalum, ceramic, film, aluminum, electrolytic, and paper dielectrics. Additional information about KEMET can be found at

Cautionary Statement on Forward-Looking Statements

Certain statements included herein contain forward-looking statements within the meaning of federal securities laws about KEMET Corporation’s (the "Company") financial condition and results of operations that are based on management's current expectations, estimates and projections about the markets in which the Company operates, as well as management's beliefs and assumptions. Words such as "expects," "anticipates," "believes," "estimates," variations of such words and other similar expressions are intended to identify such forward-looking statements. These statements are not guarantees of future performance and involve certain risks, uncertainties and assumptions, which are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in, or implied by, such forward-looking statements. Readers are cautioned not to place undue reliance on these forward-looking statements, which reflect management's judgment only as of the date hereof. The Company undertakes no obligation to update publicly any of these forward-looking statements to reflect new information, future events or otherwise.

Factors that may cause actual outcome and results to differ materially from those expressed in, or implied by, these forward-looking statements include, but are not necessarily limited to, generally adverse economic and industry conditions, including a decline in demand for the Company’s products. Other risks and uncertainties may be described from time to time in the Company’s reports and filings with the Securities and Exchange Commission.

# # #

Company Contact:Dean W. Dimke
Director of Corporate and Investor Communications