Sensor Evaluation Kit Software

Flame Sensing Evaluation Tool (Analog)

Download: flame-sensing-evaluation-tool-analog.zip

Flame Sensing Evaluation Tool for the TO Flame Sensing Evaluation Kit USEQFCK4000000. Once downloaded and unzipped, please run setup.exe file to initiate the installation process. Flame Sensing Evaluation Tool.exe will then launch the software. Further information is available in the TO Flame Sensing Evaluation Kit USEQFCK4000000 User Guide.


Flame Sensing Evaluation Tool (Digital)

Download: flame-sensing-evaluation-tool-digital.zip

Flame Sensing Evaluation Tool for the SMD Flame Sensing Evaluation Kit USEQFSK1000000 or the TO Flame Sensing Evaluation Kit USEQFCK9000000. Once downloaded and unzipped, please run setup.exe file to initiate the installation process. Flame Sensing Evaluation Tool.exe will then launch the software. Further information is available in the SMD Flame Sensing Evaluation Kit USEQFSK1000000 User Guide or the TO Flame Sensing Evaluation Kit USEQFCK9000000 User Guide.


Gas Sensing Evaluation Tool (Analog)

Download: gas-sensing-evaluation-tool-analog.zip

Gas Sensing Evaluation Tool for the TO CO2 Gas Sensing Evaluation Kit USEQGCK5000000. Once downloaded and unzipped, please run setup.exe file to initiate the installation process. Demo_Gas_TO.exe will then launch the software. Further information is available in the TO CO2 Gas Sensing Evaluation Kit USEQGCK5000000 User Guide.


Gas Sensing Evaluation Tool (Digital)

Download: gas-sensing-evaluation-tool-digital.zip

Gas Sensing Evaluation Tool for the SMD CO2 Gas Sensing Evaluation Kit USEQGSK3000000. Once downloaded and unzipped, please run setup.exe file to initiate the installation process. Gas Sensing Evaluation Tool.exe will then launch the software. Further information is available in the SMD CO2 Gas Sensing Evaluation Kit USEQGSK3000000 User Guide.


Gesture & Motion Evaluation Tool

Download: gesture-motion-evaluation-tool.zip

Gesture & Motion Sensing Evaluation Tool for the SMD Motion Sensor with Fresnel Lens Evaluation Kit USEQMSKL011600, SMD Directional Motion Sensor with Fresnel Lens Evaluation Kit USEQMSKL221600,, SMD Long-Range Motion Sensor with Fresnel Lens Evaluation Kit USEQMSKS221600, and/or the Medium-Range Motion Sensor without Optics Evaluation Kit USEQMSK1220900. Once downloaded and unzipped, please run setup.exe file to initiate the installation process. GestureDemo 2x2.exe will then launch the software. Further information is available in the SMD Gesture & Motion Sensing Evaluation Kits USEQMSK_____00 User Guide.


Linear Array Evaluation Tool

Download: linear-array-evaluation-tool.zip

Linear Array Evaluation Tool for the Base Level Evaluation Kit with Microprocessor-controlled Motherboard USEQDAK6000000, Fixed Sensor Evaluation Kits for ATR-based Spectroscopy USEQDAK7000000, USEQDAK7128L00, and USEQDAK7128500, and/or the Fixed Sensor Evaluation Kits for Transmission-Based Spectroscopy USEQDAK8000000, USEQDAK8128L00, and USEQDAK8128500. Once downloaded and unzipped, please run setup.exe file to initiate the installation process. Linear Array Evaluation Tool.exe will then launch the software. Further information is available in the Linear Array Evaluation Kits USEQDAK_____00 User Guide.


Sensor Evaluation Tool

Download: sensor-evaluation-tool.zip

Sensor Evaluation Tool Software for Control Board USEQCSK0000000. The software can be used to test up to four single-pixel sensors or one 2x2 array sensor. It enables the user to optimize the sensor for a particular environment, observe signals in real-time and to experiment with register settings. Once downloaded and unzipped, please run setup.exe file to initiate the installation process. Sensor Evaluation Tool.exe will then launch the software. Further information is available in the Sensor Evaluation Tool Software User Manual and can be used in conjunction with the SMD Sensor Reference Manual.


sKEMLIB API Driver Library

Download: skemlib-v1.0.6.zip

The sKEMLIB1 Application Programming Interface (API) is an embedded driver library for implementing KEMET environmental sensor (SMD and TO) devices. The IRPyro API provides a consistent set of functions to communicate with one or multiple IR pyroelectric sensors. The functions have been designed to be independent of the type of circuit board or microcontroller used to make the code portable to other platforms.